podis® LED 2000 Lumen

With its new, high-intensity lamp, Wieland is adding lighting components for work areas and workstations in machines and equipment to its podis® LED product line.
The podis® LED lighting components from Wieland are especially well-suited for use in industrial surroundings. Their rugged rugged and durable design ensures a high level of reliability when used in equipment. The high quality of the light from the lamps is extremely important for fast, concentrated work in work areas with particular hazards. A new feature of this lamp is the ability to select between different light distribution curves.
A lamp with a very wide light cone is extremely well-suited for uniform illumination of workstations where reflected light must be used, e.g. the nacelle of a wind turbine. A lamp with a directed light cone is beneficial efficient lighting is required along the length of a room. This may be the case when ascending towers and shafts, as well as in passageways and corridors that must be illuminated in emergency situations, for instance.
These lamps are available on a flat cable for the podis® installation platform, and also the gesis® RST® round cable energy bus.
Features of the podis® LED 2000 lm:
• spherical or oval light cone
• optimized for work areas, or escape routes, shafts, towers, totals
• glare- and flicker-free light
• efficient light source
• rugged design
• maintenance-free, extremely durable
• corrosion-resistant