• 21.02.2020
From the idea to implementation and delivery to the construction site: smart system distributors make buildings sustainable and flexible

Buildings are not short-lived products, but a long-term investment for the future. Sustainable construction is therefore important and also means correctly planning and exploiting the potential of a building over its entire life cycle from the very beginning. The more flexible the use of a building, the more sustainable. Decentralised installation of building automation and MSR electronics helps here. At the Light + Building trade fair in Frankfurt, Wieland Electric is showing plug-in system distributors which can be used to divide up individual rooms or entire floors again and again. 

 

Decentralized installation in modern building automation

Too hot, too cold, too bright, kind of stuffy? Whether we feel comfortable in a room or not has a lot to do with the temperatures, light and air conditions prevailing there. In modern buildings, heating, air conditioning and lighting are therefore intelligently controlled and individualised according to areas.
The greatest possible flexibility is achieved if the technology for this is installed decentrally, if the floor distribution only supplies the system distributors, which then use short lines to detect sensors and supply terminal devices. A major advantage for planning: these simple line structures can be easily duplicated for additional floors. 

Tailor-made system distributors for every requirement

Wieland Electric offers system distribution boards and accompanies you from the initial concept to the finished installation - whether in small or large buildings, office complexes or warehouses. There are hardly any limits to the variants and areas of application because all Wieland system distributors are individually manufactured according to customer requirements. The size, material and surface of each distribution board can be selected according to the project requirements, and the electronics of all trades can be integrated: From the terminal block to the room controller. All distributors are equally suitable for wall, ceiling and floor mounting.

Pluggability ensures speed and flexibility

As with all other Wieland products, the system distributor scores with the principle " plugging instead of screwing“. Color-coded and mechanically coded plug connectors ensure fast and error-free connection and can be easily and flexibly adapted to subsequent changes in use

Wieland at the Light + Building in Frankfurt

Wieland Electric will present the complete "system distributor" package - from the idea to implementation and delivery to the construction site – at the Light + Building trade fair from 27 September to 02 October (Hall 12, Stand B60, Hall 8, Stand C50) in Frankfurt.

DOWNLOADS

Press Release Distribution Boxes

2 MB

Systemverteiler_distribution-box.jpg

91 KB

Corporate - English
Industries
BackIndustriesAll IndustriesBuilding TechnologyLighting TechnologyMachine BuildingWind Power
Products
BackProductsElectrical InstallationConnection TechnologySafety TechnologyIndustrial CommunicationElectronic + Interface
Support
BackSupportServiceSoftware & AppsInfoportalDownloadsTraining
Company
BackCompanyAbout usPurchasing & QualityNewsCareer