DIN rail terminal blocks
DIN rail terminal blocks organise and distribute power and signals within control cabinets and electrical systems. Choose between modern Push-in and screw connection technologies, functional terminal types, marking solutions and compatible accessories for efficient installation, dependable contact and clear circuit identification.
LOOKING FOR A CONNECTION?
CONNECTION TECHNOLOGIES FOR TERMINAL BLOCKS
Terminal blocks are electromechanical components used in control cabinets or circuit distribution panels to connect wires, cores, and cables in a detachable and safe manner. When clamped, they distribute power or electrical signals within the control cabinet via a lead.
Terminal blocks are mounted side by side on DIN rails and installed in the control cabinet. Incoming and outgoing conductors from other electrical components or devices are connected to the terminals of the terminal blocks, integrating them into a complex overall system. The essential task of terminal blocks in electrical engineering is to connect electrical conductors and, for example, to control or monitor building installations, power engineering, machines, and systems.
Terminal blocks are used for the connection of conductors at junctions of power and control circuits in power distribution or for the signal distribution of sensors and actuators. The blocks are typically used in control cabinets, where they are mounted on terminal or DIN rails.
They are differentiated as follows:
- Terminal blocks with small nominal cross section (1.5 mm² and 2.5 mm²), primarily used for sensor signal distribution.
- Terminal blocks with a nominal cross section of 4 mm² or 6 mm²; they are mostly used as terminal blocks for actuators such as pneumatic cylinders, electric motors, and similar.
- Terminal blocks with a nominal cross section of 10 mm² and more are often used for power distribution at higher voltage levels.
In principle, there is no universally applicable legal obligation in Germany to use terminal blocks. However, there are exceptions for special applications—such as the construction of electrical installations in fire-hazardous workplaces. According to DIN VDE 0105-100/A1, electrical installations must be repeatedly tested. An essential test aspect is the so-called insulation measurement, e.g., between neutral conductor and yellow/green conductor. For this measurement, it is necessary to disconnect the neutral conductor of each circuit. Therefore, DIN VDE 0100-718 and VdS 2033 require the use of N-disconnect terminal blocks in public facilities, commercial or industrial workplaces, and fire-hazardous workplaces.
How many terminal blocks you can place at most on a DIN rail (top hat rail) depends on terminal type, connection technology, and conductor cross-section. In practice, it is often neither sensible nor necessary to push the theoretically possible maximum number of terminal blocks on a terminal strip to the limit. A structured layout with sufficient clearances is better. This makes assembly and modification, maintenance, and inspection easiest, and keeps things clear in the control cabinet.