EN | International
  • International | English
  • Česko | Čeština
Contact
  • International | English
  • Česko | Čeština
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
Modernize electrical installations in existing buildings

Whether refurbishment, renewal or revitalization: with pluggable installation systems, you make existing buildings ready for today’s requirements and future usage concepts – easy to plan, economical, and with minimal intervention in the building fabric.

Request a consultation

The building stock 
is under pressure

A large proportion of buildings are over 30 years old—and so are their electrical installations. At the same time, demands are increasing: flexible space concepts, energy efficiency, digitalization, as well as applications such as e-mobility or Photovoltaic.

Many existing electrical installations are not designed for these demands. They offer too little reserve for modern applications, are often undersized, not very flexible, and no longer meet the safety and comfort standards of contemporary buildings.

Those who only make selective renewals in existing buildings often merely solve acute problems. A building becomes future-proof only when the electrical installation is considered structurally.

Renewing the electrical installation in existing buildings is not just a technical measure—it determines how safe, usable, and future-proof a building remains.

More than THE electrical refurbishment OF OLD WIRING

Revitalization means not only modernizing existing buildings, but making them usable and adaptable in the long term. It’s not just about replacing old electrical wiring. The key is an electrical installation that meets today’s requirements and takes future changes into account.

The focus is on a solution that:

  • establishes an up-to-date level of safety
  • reliably supplies modern applications
  • reduces interventions in the building fabric
  • enables short construction times during ongoing operations
  • can be flexibly expanded and adapted

The crucial difference: an installation that not only works for today—but also remains adaptable tomorrow.

EVERY REVITALIZATION BRINGS CHALLENGES WITH IT 
– WE DELIVER THE RIGHT SOLUTION

When renewing the electrical installation in existing buildings, every intervention counts. Construction times, the building fabric, and later changes in use must be considered from the outset. with pluggable systems, this becomes a plannable solution: less effort on site, less intervention in the building fabric, and more flexibility for later changes.

The following examples show how typical challenges of revitalization can be solved efficiently.

Operations & Time Pressure
Existing Building Structure
On-Site Installation Errors
Safety in Existing Buildings
Flexibility in the Building
Future & Sustainability

ONGOING OPERATIONS & TIME PRESSURE

Challenge:

Revitalizations often take place during ongoing operations—for example, in offices, hotels, educational institutions, or residential complexes. The more the building fabric is interfered with, the greater the downtime, disruptions, and costs.

Requirement:

The modernization must be carried out so that operational interruptions are reduced to a minimum—while ensuring high predictability and execution reliability.

Solution:

  • Pluggable systems enable installation up to 70% faster through plug & play instead of individual wiring
  • Prefabricated, tested components significantly reduce assembly effort and sources of error

Modernization must adapt to operations—not the other way around.

Result:

Buildings remain largely usable—and are back in full operation much faster.

→ Pluggable solutions in action

Expert assessment: 
Why modern electrical installation is crucial

“Renewing the electrical installation in existing buildings is not a replacement of old technology, but the foundation for safety, usability, and future readiness.”

Dominik Stöcklein 
Product Manager gesis®

CONVENTIONAL VS. PLUGGABLE: THE DIFFERENCE AT A GLANCE

Pluggable installation systems not only offer conceptual advantages, they also have a measurable impact on time, costs, and material usage.

Conventional Electrical Installation
Pluggable Installation with Wieland
Time required
Costs
Cable lengths
Fire load
Copper weight
Technical rooms

The values shown are based on typical project comparisons and may vary depending on the application.

SUSTAINABLE ELECTRICAL INSTALLATION 
BEGINS IN EXISTING BUILDINGS

Revitalization is a key lever for sustainable construction—because most of the buildings of tomorrow already exist today.

For these buildings to remain energy-efficient, flexible, and certifiable in the long term, the electrical installation must be considered from the ground up.

FROM INCREASING REQUIREMENTS TO A FUTURE-PROOF ELECTRICAL INSTALLATION

REQUIREMENTS FOR EXISTING BUILDINGS

Energy efficiency is no longer an optional goal today, but enshrined in law—for example through the Building Energy Act (GEG) or DIN 18599. For electrical engineering, this means concrete requirements, e.g., through daylight-dependent lighting control.

At the same time, green building certifications such as DGNB, LEED, or BREEAM are becoming increasingly important. They assess buildings holistically—from energy efficiency and resource use to flexibility and utilization.

CONTRIBUTION OF PLUGGABLE SYSTEMS

This is exactly where pluggable, modular systems come in. They support the implementation of sustainable building concepts in two ways:

  • They meet the increasing requirements for energy efficiency and enable the easy integration of modern building technology
     
  • At the same time, they create measurable benefits for certifications—such as through lower material usage, reusability, and flexible use

This makes the electrical installation in existing buildings the decisive lever for sustainable buildings: it makes requirements for energy efficiency, certifiability, and flexible use technically feasible.

RESOURCE CONSERVATION

Fewer interventions in the building fabric reduce material usage and construction effort.

  • fewer interventions in the building fabric
  • lower material usage
  • reduced construction waste

CIRCULAR ECONOMY

Reusable systems avoid unnecessary deconstruction and enable long-term use.

  • reusable plug-in systems
  • non-destructive adaptation and expansion
  • less “throw away and start over”

ENERGY EFFICIENCY

A modern electrical installation forms the foundation for energy-efficient building technology.

  • Foundation for modern building technology
  • Integration of LED, smart building, and load management

REFURBISHMENT OF THE ELECTRICAL INSTALLATION IN PRACTICE

As diverse as buildings are, so too are the requirements for their revitalization. Discover suitable solutions for your application.

Revitalization begins 
with good planning

Before an electrical installation in an existing building is renewed, a clear assessment of the existing conditions is needed: Which cable routes are in place? Which loads need to be supplied? What requirements arise from new usage concepts, building services, or future expansions?

Wieland supports you in developing a plannable system solution from these requirements—with pluggable components that reduce construction time, minimize interventions, and make future adjustments easier.

→ Plan the design together

THE RIGHT INSTALLATION SYSTEMS FOR THE 
RENEWAL OF YOUR ELECTRICAL INSTALLATION

With pluggable systems and modular components, Wieland Electric offers a seamless portfolio for the efficient and future-proof renewal of electrical installations in existing buildings.

FLAT CABLE SYSTEM FOR EFFICIENT POWER DISTRIBUTION

With the gesis® NRG flat cable system, you reduce cabling effort by up to 70%. Less material, lower fire load, and maximum flexibility—ideal for office, education, and healthcare buildings.

→ Discover the flat cable system

DISTRIBUTION BOX FOR 
POWER AND DATA

The gesis® RAN distribution box enables decentralized power and data distribution for modern building structures. Quick to install, flexibly extendable, and reliable in operation.

→ Discover distribution box

PLUGGABLE CONNECTION TECHNOLOGY FOR EVERY APPLICATION

With the gesis® installation system, you create reliable connections for lighting, power supply, and control—from individual applications to the complete electrical installation.

→ Discover installation connectors

FAQ

What should be considered when renewing the electrical installation in existing buildings?

Early planning, a thorough assessment of the existing conditions, and sufficient flexibility for later changes in use are important. Straight in existing buildings, cable routes, spatial constraints, safety requirements, and future applications such as smart building, LED lighting, or charging infrastructure should be considered from the outset.

How can we avoid having to renew the electrical installation again in 30 years?

By not understanding the renewal as a one-time refurbishment, but as the Setup of an adaptable infrastructure. Conventional installations are often rigid and can only be modified with considerable effort.

Pluggable installation systems, on the other hand, enable later expansions, repurposing, or adaptations with significantly fewer interventions. This means the electrical installation is not only suited to today’s requirements, but can be developed further with the building.

Contact

Are you planning to revitalize your electrical installation?

Speak with our specialists and find the right solution for your project.

Call now at: +49 951 9324 996

Send inquiry
CALLBACK – SERVICE

Get personalized advice—quickly and easily.

Our experts support you in the planning and implementation of your revitalization.

  1. Fill out the form
  2. Specify preferred date
  3. Receive a callback
Schedule a consultation

Our eShop has moved

Our website and eShop are now combined on one platform. Product information and shop features are now available directly here. Use the search or select a product category.

Already have a customer account? Please follow the instructions when signing in.

Need assistance? Contact our eShop support team by email at ebusiness@wieland-electric.com.

×